DOCA0187EN-03

Plug-in Circuit Breaker

Introduction

Plug-in base circuit breakers make it possible to:

  • Extract and/or rapidly replace the circuit breaker without having to touch the connections on the base

  • Allow for the addition of future circuits by installing bases that will be equipped with a circuit breaker at a later date

  • Isolate the power circuits when the circuit breaker is mounted on or through a panel. It acts as a barrier for the connections of the plug-in base. Insulation is made complete by the mandatory short terminal shields on the circuit breaker.

The following types of circuit breaker can be installed in a plug-in base:

  • 3P and 4P circuit breakers

  • Circuit breakers with toggle handle, direct rotary handle, or extended rotary handle

  • Motor-operated circuit breakers

  • Circuit breakers with VigiPacT Add-on

NOTE: ComPacT NSX400K circuit breakers cannot be installed in a plug-in base.

The plug-in circuit breaker is made up of the fixed circuit breaker and a plug-in kit, which includes:

  • Plug-in base

  • Power connections

  • Short terminal shields

  • Safety trip interlock

For more information about plug-in circuit breaker installation, consult the instruction sheets on the Schneider Electric website:

Plug-in Kit and Chassis Installation Demonstration Video

To access a demonstration video about the installation of a plug-in kit and chassis for withdrawable ComPacT NSX100-250 circuit breakers, click the following link: https://youtu.be/XaXO6QgeWvM, copy and paste the link to your Web browser, or scan the QR code.

Disconnecting the Circuit Breaker

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, NOM-029-STPS, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • The circuit breaker must be in the O (OFF) position.
  • Do not use tools to disconnect or connect the circuit breaker.
Failure to follow these instructions will result in death or serious injury.

Follow this procedure to disconnect the circuit beaker:

Step

Action

1

Switch the circuit breaker to the O (OFF) position.

2

Remove both mounting screws.

3

Pull out the circuit breaker, keeping it horizontal.

NOTE:
  • The auxiliary circuits automatically disconnect because of the connectors located on the base and at the rear of the circuit breaker.

  • Open the circuit breaker before disconnecting it. If the circuit breaker is in the closed I (ON) position when disconnecting, a pre-trip mechanism trips the circuit breaker before the pins are disconnected.

Connecting the Circuit Breaker

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, NOM-029-STPS, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • The circuit breaker must be in the O (OFF) position.
  • Do not use tools to disconnect or connect the circuit breaker.
Failure to follow these instructions will result in death or serious injury.

Follow this procedure to connect the circuit beaker:

Step

Action

1

Switch the circuit breaker to the O (OFF) position.

2

Connect the circuit breaker.

3

Replace both mounting screws. Tighten the screws to a torque of 2.5 N•m (22.1 lb-in).

NOTE:
  • The auxiliary circuits automatically connect because of the connectors located on the base and at the rear of the circuit breaker.

  • Open the circuit breaker before connecting it. If the circuit breaker is in the closed I (ON) position when connecting, the pre-trip mechanism trips the circuit breaker before the pins are connected.

Protection Against Direct Contact With Power Circuits

The following table shows plug-in circuit breaker configurations with the corresponding protection indices (IP):

Configuration

Protection index

Description

IP20

Built-in plug-in base:

  • Without circuit breaker

  • With circuit breaker without terminal shields

IP40

Built-in plug-in base and circuit breaker with terminal shields.

IP40

Plug-in base with adapter, terminal shields and blanking plate without circuit breaker:

  • The adapter enables the use of all the connection accessories of the fixed circuit breaker. It is required to equip the plug-in circuit breaker with long and short terminal shields and interphase barriers.

  • Terminal shields are mandatory for plug-in circuit breakers. Short terminal shields are supplied in the plug-in kit. They can be replaced by long terminal shields available as an option.

  • The blanking plate is not supplied by Schneider Electric.

IP40

Plug-in base with adapter and terminal shields, and circuit breaker with terminal shields.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.