DOCA0187EN-03

Electrical Auxiliary Device Summary

Electrical Auxiliary Devices

The following table shows the electrical auxiliary devices that can be added to the ComPacT NSX circuit breakers. For more information, refer to LVPED221001EN ComPacT NSX & NSXm Catalogue.

Electrical auxiliary device

NSX100

NSX160

NSX250

NSX400

NSX630

1P

2P

3P/4P

1P

2P

3P/4P

1P

3P/4P

3P/4P

3P/4P

OF or SD auxiliary contact

SDE auxiliary contact

SDx module

SDTAM module

Wireless indication auxiliary

MN undervoltage trip release

MX shunt trip release

BSCM Modbus SL/ULP module

SD auxiliary contact for BSCM Modbus SL/ULP module

NSX cord

24 Vdc power supply connector(1)

(1) with MicroLogic 5, 6, and 7 trip units

Electrical Auxiliaries Installation Demonstration Video

To access a demonstration video about the installation of electrical auxiliary devices in a ComPacT NSX100-250 3P circuit breaker, click the following link: https://youtu.be/zDqRyZHBWr4, copy and paste the link to your Web browser, or scan the QR code.

Slots for Electrical Auxiliary Devices on ComPacT NSX100/160 2P Circuit Breakers

The following table shows the possible slots for electrical auxiliary devices mounted in the case. Only one auxiliary device can be installed per slot. For more information, refer to LVPED221001EN ComPacT NSX & NSXm Catalogue.

Name

Slot

A

B

C

OF1 (wired or wireless)

SD (wired or wireless)

MN

MX

Slots for Electrical Auxiliary Devices on ComPacT NSX100-250 3P/4P Circuit Breakers

The following table shows the possible slots for electrical auxiliary devices mounted in the case. Only one auxiliary device can be installed per slot. For more information, refer to LVPED221001EN ComPacT NSX & NSXm Catalogue.

Name

Slot

 

Comments

A

B

C

D

E

F

Standard indication and control auxiliaries

OF1 (wired or wireless)

For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism).

OF2 (wired or wireless)

SD (wired or wireless)

SDE (wired or wireless)

SDV (wired only)

Indication contact in VigiPacT Add-on

MN

For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism).

MX

Remote indication and communication auxiliaries

BSCM Modbus SL/ULP module

SD auxiliary contact for BSCM Modbus SL/ULP module

Compatible with the BSCM Modbus SL/ULP module in Modbus SL only mode.

NSX cord

For connection of the BSCM Modbus SL/ULP module to ULP modules.

NSX cord

For connection of MicroLogic 5, 6, and 7 trip units to ULP modules when no BSCM Modbus SL/ULP module is installed.

Specific indication auxiliaries with MicroLogic trip units

SDx

Including SDV for MicroLogic 4 and 7 trip units.

SDTAM

Only for circuit breakers with a MicroLogic 2 M or 6 E-M trip unit designed to protect motors.

24 Vdc power supply connector

For connection of external power supply to MicroLogic 5, 6, and 7 trip units.

NOTE: It is not possible to install all the auxiliaries at the same time on one trip unit. For example, the SDx module cannot be installed at the same time as an MN or MX release and the OF1 contact.

Slots for Electrical Auxiliary Devices on ComPacT NSX400-630 3P/4P Circuit Breakers

ComPacT NSX400-630 circuit breakers are exclusively equipped with MicroLogic trip units.

The following table shows the possible slots for the electrical auxiliary devices mounted in the case. For more information, refer to LVPED221001EN ComPacT NSX & NSXm Catalogue.

Name

Slot

Comments

A

B

C

D

E

F

G

H

I

Standard indication and control auxiliaries

OF1 (wired or wireless)

For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism).

OF2 (wired or wireless)

OF3 (wired or wireless)

OF4 (wired or wireless)

SD (wired or wireless)

SDE (wired or wireless)

SDV (wired only)

Indication contact in VigiPacT Add-on

MN

For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism).

MX

Remote indication and communication auxiliaries

BSCM Modbus SL/ULP module

SD auxiliary contact for BSCM Modbus SL/ULP module

Compatible with the BSCM Modbus SL/ULP module in Modbus SL only mode.

NSX cord

For connection of the BSCM Modbus SL/ULP module to ULP modules.

NSX cord

For connection of MicroLogic 5, 6, and 7 trip units to ULP modules when no BSCM Modbus SL/ULP module is installed.

Specific indication auxiliaries with MicroLogic trip units

SDx

Including SDV for MicroLogic 4 and 7 trip units.

SDTAM

Only for circuit breakers with a MicroLogic 2 M or 6 E-M trip unit designed to protect motors.

24 Vdc power supply connector

For connection of external power supply to the MicroLogic 5, 6, and 7 trip units.

NOTE: It is not possible to install all the auxiliaries at the same time on one trip unit. For example, the SDx remote indication option cannot be installed at the same time as an MN or MX release.

Operation of the Indication Contacts

The following table shows the position of the indication contacts (or outputs) relative to the position of the actuator and main contacts.

 

Position of the actuator and the main contacts

ON

Tripped by:

OFF

MN/MX

PT(1)

Trip unit(2)

L

S or So

I

R

G

Name

Position of indication contacts

OF

SD

SDE

SDV

SDx outputs(3)

SD2

SDT

SD4

PAL

SDG

SDV

SDTAM outputs

SD2

Early make/break SDT

✔✔

SD4

Contactor control

: Contact closed, ✔✔: Early-make output (400 ms)

(1) PT: Push-to-trip

(2) L: Long-time protection

S or So: Short-time protection

I: Instantaneous protection

R: VigiPacT Add-on protection (earth-leakage)

G: Ground-fault protection

(3) SDx output assignment can be customized for MicroLogic 5, 6, and 7 trip units, by using EcoStruxure Power Commission software.

NOTE: The indication (changeover) contacts are represented in the switchboard by the state of the Normally Open (NO) contact.

The state of the NO contact is open:

  • for OF contacts when the circuit breaker is in the O (OFF) position.

  • for SD, SDE, and SDV contacts when the associated function is not active.

Sequence chart of the OF contacts relative to the main contacts

A Main contacts

B Position of OF changeover contacts

Operation of the Wireless Indication Auxiliaries

The wireless indication auxiliary provides the same information as a standard wired auxiliary contact in OF, SD, or SDE positions. The information is sent remotely to a gateway or Panel Server.

During commissioning of the wireless indication auxiliary, the user defines the type of information sent: Open/Close or Trip.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.