DOCA0187EN-03

ComPacT NSX100-250 - Distribution Protection Tripping Curves

TMD Magnetic Trip Units

For all TMD curves:

Values are given for 40 °C ambient, Ir = 1 x In, 3 poles loaded, cold start.

For Ir = k x In, read the time corresponding to 1/k times given current.

For 1 pole tripping, read the time corresponding to 0.85 times given current.

For hot start (0.9 x Ir), divide max. time by 2, min. time by 4.

TM16D

Reflex tripping

TM25D

TM32D

Reflex tripping

TM40D

TM50D

Reflex tripping

TM63D

TM80D / TM100D

Reflex tripping

TM125D / TM160D

TM200D / TM250D

Reflex tripping

TMG Magnetic Trip Units

TM16G

Reflex tripping

TM25G

TM40G

Reflex tripping

TM63G

TM80G

Reflex tripping

TM100G

TM125G

Reflex tripping

TM160G

TM200G

Reflex tripping

TM250G

MicroLogic 2.2 and 4.2 Electronic Trip Units

MicroLogic 2.2 and 4.2 - 40–160 A

Reflex tripping

MicroLogic 2.2 and 4.2 - 250 A

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.