DOCA0187EN-03

MicroLogic 2 M Electronic Trip Unit

Introduction

The MicroLogic 2 M electronic trip unit is suitable for protecting motor-feeders on standard applications. The thermal trip curves are calculated for self-ventilated motors.

The MicroLogic 2 M electronic trip unit can be used to create a type 1 or type 2 coordination motor-feeder.

Description

The adjustment dials and indications are on the front face.

MicroLogic 2.2 M

A MicroLogic electronic trip unit setting range

B Adjustment dial for the long-time protection pickup Ir

C Selection dial for the long-time protection time delay class

D Adjustment dial for the short-time protection pickup Isd

E Value of instantaneous protection pickup Ii

F Test port

G Ready LED (green)

H Alarm LED

I Phase-unbalance

The trip unit rating In corresponds to the maximum value of the setting range.

Setting the Long-Time Protection

The long-time protection is set by 2 dials according to the starting characteristics of the application.

  • The long-time protection pickup Ir is set using a multi-position dial.

    The maximum setting value (maximum setting on adjustment dial) equals the trip unit rating value In.

The following table shows the values of the pickup Ir (in amperes) for long-time protection that are displayed directly on the dial with respect to every trip unit rating.

Trip unit rating In (A)

25

50

100

150

220

320

500

Pickup Ir (A)

12

25

50

70

100

160

250

14

30

60

80

120

180

280

16

32

70

90

140

200

320

18

36

75

100

155

220

350

20

40

80

110

170

240

380

22

42

85

120

185

260

400

23

45

90

130

200

280

440

24

47

95

140

210

300

470

25

50

100

150

220

320

500

  • The long-time protection time delay class is set by using a multi-position dial: the choice of class is 5, 10 and 20.

The following table shows the value of the trip time delay depending on the current in the load for all 3 classes:

Current in the load

Class

5

10

20

Trip time delay tr (in seconds)

1.5 x Ir

120

240

400

6 x Ir

6.5

13.5

26

7.2 x Ir

5

10

20

The precision range is - 20%, + 0%.

Setting the Short-Time Protection

The pickup for short-time protection is set by using a multi-position dial. It is displayed in multiples of Ir

Step

Action

1

Set the long-time protection first: the setting pickup is Ir (A).

2

Turn the Isd adjustment dial to the value required (the setting range is: 5 to 13 x Ir in steps of Ir (9 settings)).

3

Isd is set to Ir (A) x Isd setting.

The precision range is +/- 15%.

The short-time protection time delay cannot be adjusted: 30 ms.

Setting the Instantaneous Protection

The following table shows the pickup Ii values (in amperes) according to the trip unit rating In.

 

Trip unit rating In (A)

25

50

100

150

220

320

500

Pickup Ii (A)

425

750

1500

2250

3300

4800

7500

The precision range is +/- 15%.

Phase-Unbalance Protection

MicroLogic 2 M trip units incorporate a protection against phase-unbalance. The characteristics are:

  • Protection not adjustable

  • Pickup: 30% phase-unbalance (the precision range is +/- 20%)

  • Overshoot time: 4 s in steady state, 0.7 s during startup

Example: A phase-unbalance exceeding 30% for longer than 4 s in steady state causes the protection to trip.

Contactor Opening Command

Trip units fitted with an SDTAM module can use output 2 (SD4) from this module to activate the contactor opening command for the motor-feeder before the circuit breaker trips.

Example of Application

Protection of a motor-feeder with the following characteristics:

  • Power supplied by a 1,250 kVA transformer - 400 V, 4%

  • Protection of a motor application defined by:

    • 2-component motor-feeder (circuit breaker, contactor)

    • Direct-on-line starting

    • Motor power 110 kW, that is, In = 196 A

    • Type 2 coordination

    • The application constraints dictate a slow startup

Installation diagram

Calculations performed on the installation in accordance with the regulations have determined the characteristics of the appropriate ComPacT NSX to install (calculations performed using the Ecostruxure Power Design – Ecodial software).

Installation diagram

Installation

Chosen ComPacT NSX

Comments

In = 196 A

ComPacT NSX250

MicroLogic 2.2 M 220

Motor circuit breaker, case size

Isc = 28.5 kA

F

Icu performance can be read from rating plate

Ik min = 14.8 kA

Trip unit protection settings

Installation

Trip unit setting

Comments

In = 196 A

MicroLogic 2.2 M 220 set to 200 A

MicroLogic trip unit setting

Slow starting

Set in class 20

Long-time protection trip class

Ik min = 14.8 kA

Transient = 14 In

Isd/In > 12 or Isd > 2,400 A

Isd protection setting compatible with:

  • Transient startup currents

  • Short-circuit protection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.