DOCA0187EN-03

BSCM Modbus SL/ULP Module Presentation

The BSCM Modbus SL/ULP module with commercial reference LV434220 is a Breaker Status Control Module that can be used to communicate data via:

  • Modbus Serial Line communication network

  • ULP communication network

Use the BSCM Modbus SL/ULP module with:

  • ComPacT NSX circuit breakers equipped with:

    • Thermal-magnetic trip units

    • MicroLogic electronic trip units

  • ComPacT NSX switch-disconnectors

NOTE: The BSCM Modbus SL/ULP module cannot be installed in a ComPacT NSX400K circuit breaker.

The following data is exchanged:

  • OF and SDE circuit breaker states from the BSCM Modbus SL/ULP module

  • SD circuit breaker state from SD auxiliary contact for BSCM Modbus SL/ULP module or NSX cord (if present)

  • Control instructions for the communicating motor mechanism (if present): opening, closing, and resetting

  • Information to assist the operator: storage of the last 10 events

When connected to a MicroLogic 5, 6, or 7 trip unit, the BSCM Modbus SL/ULP module gives access to MicroLogic data.

For more information about integrating ComPacT NSX circuit breaker communication functions, refer to:

Description of the BSCM Modbus SL/ULP Module

  1. Port for BSCM Modbus SL cord

  2. Modbus address selector rotary switch

  3. Port for communicating motor mechanism

  4. ULP status LED

  5. Modbus status LED

  6. Port for MicroLogic 5, 6, or 7 trip unit

  7. Port for NSX cord or SD auxiliary contact for BSCM Modbus SL/ULP module

  8. OF contact

  9. SDE contact

  10. Cable to connect the BSCM Modbus SL/ULP module to the NSX cord or SD auxiliary contact for BSCM Modbus SL/ULP module

  11. Cable to connect the BSCM Modbus SL/ULP module to a MicroLogic 5, 6, or 7 trip unit

ULP LED Indication on BSCM Modbus SL/ULP Module

The ULP LED provides indications on the state of the BSCM Modbus SL/ULP module, even in Modbus SL only mode.

The ULP LED color on the BSCM Modbus SL/ULP module is yellow.

ULP LED

Mode

Action

Nominal

None

Conflict

Remove extra ULP module

Degraded

Replace the BSCM Modbus SL/ULP module at the next maintenance operation

Test

None

Non-critical firmware discrepancy

Upgrade firmware at the next maintenance operation

Non-critical hardware discrepancy

Replace the BSCM Modbus SL/ULP module at the next maintenance operation

Configuration discrepancy

Install missing features

Critical firmware discrepancy

Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions

Critical hardware discrepancy

Stop

Replace the BSCM Modbus SL/ULP module

Power off

Check power supply

Modbus Serial Line LED Indication on BSCM Modbus SL/ULP Module

The Modbus Serial Line LED color on the BSCM Modbus SL/ULP module is white.

The LED status is as follows:

  • Off: the Modbus Serial Line communication network is disabled.

  • On steady: the Modbus Serial Line communication network is enabled.

  • Blinking: the Modbus Serial Line communication is ongoing.

Installing the BSCM Modbus SL/ULP Module

The slots used to install the BSCM Modbus SL/ULP module depend on the circuit breaker type.

ComPacT NSX100-250

ComPacT NSX400-630

A BSCM Modbus SL/ULP module

B NSX cord or SD auxiliary contact for BSCM Modbus SL/ULP module

The BSCM Modbus SL/ULP module cannot be installed at the same time as an OF contact or the SDE contact.

The BSCM Modbus SL/ULP module can be installed on site.

For more information about installation, consult the instruction sheet on the Schneider Electric website: PKR1891407 ComPacT NSX100–630 – BSCM Modbus SL/ULP.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.