DOCA0187EN-03

TM-D Thermal-Magnetic Trip Unit for 1P Circuit Breakers 250 A

Introduction

TM-D thermal-magnetic trip units for 1P circuit breakers 250 A are built-in trip units.

They are designed for AC applications.

TM-D built-in 1P trip units provide:

  • fixed thermal threshold

  • fixed magnetic pickup

Setting the Thermal Protection

The thermal protection pickup Ir cannot be adjusted and equals the value shown below:

Trip unit rating In (A) at 40 °C (104 °F)

160

200

250

Fixed pickup Ir (A) at 40 °C (104 °F)

160

200

250

Setting the Magnetic Protection

The magnetic protection pickup Ii cannot be adjusted and equals the value shown below:

Trip unit rating In (A)

160

200

250

Fixed pickup Ii (A) +/– 20%

850

850

850

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.