DOCA0187EN-03

PowerTag Energy M250/M630

Introduction

PowerTag Energy M250/M630 is a class 1 energy meter, as per IEC 61557-12, that incorporates features required to perform accurate real-time measurements (U, V, I, P, PF) and get energy values up to 250 A or 630 A, depending on the model.

Used together with a gateway or a Panel Server to collect and process the data, the PowerTag Energy M250/M630 provides circuit monitoring and diagnosis down to load level.

The PowerTag Energy M250/M630 is designed for molded case circuit breakers and switch-disconnectors (ComPacT NSX and Tesys Giga - Frame 5/Frame 6) for 3P and 3P+N electrical networks.

The PowerTag Energy M250/M630 is mounted directly on the bottom side of the circuit breaker or VigiPacT Add-on if any. For a PowerTag Energy M250/M630 mounted on a plug-in base, the PowerTag Energy M250/M630 must be installed on the top or bottom of the base, depending on the configuration. For more information, refer to CA908058E PowerTag Energy Selection Guide.

Thanks to its integrated design, the PowerTag Energy M250/M630 does not require any specific wiring and is compatible with the same connection accessories as the device it is mounted on.

For more information about installation, consult the instruction sheets on the Schneider Electric website:

  • QGH46815 PowerTag Energy M250 3P/3P+N

  • QGH46820 PowerTag Energy M630 3P/3P+N

  • MFR37601 PowerTag Energy M250/M630 3P/3P+N – ComPacT NSX100-250/400-630 Plug-in Base

Description

A Status LED

B QR code to access device information including wireless address

C Switch to disconnect PowerTag Energy supply from the phases, used when performing a panel dielectric test

D Wireless address

E Neutral voltage picking (on PowerTag Energy 3P only)

Status LED

Use the LED indication to confirm that the PowerTag Energy M250/M630 is working during commissioning or maintenance operations.
Status LED Description Action

PowerTag Energy M250/M630 switched off.

None or check power supply depending on operation type.

PowerTag Energy M250/M630 searching a concentrator or gateway.

Wait until the concentrator or gateway is identified.

PowerTag Energy M250/M630 in identification mode.

Wait until PowerTag Energy M250/M630 is in network.

PowerTag Energy M250/M630 in network. Normal communication with the concentrator or gateway.

None

Occasional loss of communication.

Check communication setting with the concentrator or gateway.

Loss of communication with the concentrator or gateway.

Check communication setting with the concentrator or gateway.

Internal error detected.

Replace the PowerTag Energy M250/M630 .

Data Available

To get the list of data available, refer to the relevant gateway or Panel Server user guide. Data available depends on the gateway.

Commissioning

To commission the PowerTag Energy, refer to the user guide of the gateway or Panel Server to which the PowerTag Energy is to be paired. Commissioning is different from one gateway to another.

NOTE: Check the firmware of the gateway before performing the commissioning of PowerTag Energy M250/M630. It is recommended to upgrade to the latest version available.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?