DOCA0187EN-03

Maintaining the Circuit Breaker During Operation

Introduction

The electrical switchboard and all its equipment continue to age whether they operate or not. This aging process is due mainly to environmental influences and operating conditions.

To help ensure that circuit breaker retains the operating and safety characteristics specified in the catalogue for the whole of its service life:

  • Install the circuit breaker in optimum environmental and operating conditions (described in the following table).

  • Have routine inspections and regular maintenance done by qualified electrical personnel.

Environmental and Operating Conditions

The environmental conditions previously described refer to harsh operating environments.

The following table describes the optimum environmental and operating conditions:

Environmental and operating factor

Comments

Temperature

Average annual temperature outside the switchboard: < 25 °C (77 °F).

Loading

Loading remains < 80% of In 24 hours a day.

Harmonics

The harmonic current per phase is < 30% of In.

Humidity

The relative humidity is < 70%.

Corrosive atmosphere (SO2, NH3, H2S, Cl2, NO2)

Install the circuit breaker in environmental category 3C1 or 3C2 (IEC/EN 60721-3-3).

Saline environment

Install the circuit breaker in an environment free of salt mist.

Dust

The dust level is low: protect the circuit breaker within a switchboard fitted with filters or IP 54 ventilated.

Vibration

Continuous vibration is < 0.2 g.

The maintenance programs apply to optimum environmental and operating conditions. Outside these limits circuit breakers are subject to accelerated aging which can quickly lead to malfunctions.

Regular Preventive Maintenance

Maintenance recommendations for each device are intended to maintain the equipment or subassemblies in a satisfactory operational state for their useful service life.

There are three recommended preventive maintenance programs:

  • Basic end-user maintenance program

  • Standard end-user maintenance program

  • Manufacturer maintenance program

NOTE: Global service plans delivered by Schneider Electric may include maintenance plans for your equipment, with a different wording for maintenance levels:
  • Basic end-user maintenance in this guide corresponds to Routine maintenance in service plans.

  • Standard end-user maintenance in this guide corresponds to Intermediate maintenance in service plans.

  • Manufacturer maintenance remains the same.

The following table summarizes maintenance operations for the three preventive maintenance programs:

Maintenance program

Maintenance description

Performed by

Basic end-user maintenance

Visual inspection and functional testing, replacement of inoperative accessories.

  • Trained and qualified end-user personnel

  • Trained and qualified maintenance services provider personnel

  • Schneider Electric field service representative

Standard end-user maintenance

Basic end-user maintenance, plus operational servicing and subassembly tests.

  • Trained and qualified maintenance services provider personnel

  • Schneider Electric field service representative

Manufacturer maintenance

Standard end-user maintenance, plus diagnostics and part replacements by Schneider Electric Services.

Schneider Electric field service representative

If all environmental conditions are more favorable than normal, maintenance intervals can be longer than the ones in normal environmental and operating conditions (for example, Standard end-user maintenance programs can be carried out every 3 years).

If any one of the conditions is more severe, perform maintenance more frequently. For advice, contact Schneider Electric Services.

Functions linked specifically to safety require particular maintenance intervals.

NOTE: Regularly test that the remote safety commands work. For example, test at least every six months.

Maintenance Operations Required

CAUTION
HAZARD OF EQUIPMENT DAMAGE
Insulation and dielectric strength tests must only be carried out by qualified electrical personnel.
Failure to follow these instructions can result in injury or equipment damage.

Maintenance operation mainly consists of checks and inspections A, D, E, F, G, I, and J as defined for the commissioning phase.

Letter - maintenance operation

Maintenance operation

Year 1

Year 2

Year 3

Year 4

Year 5

A

Insulation and dielectric strength tests

D

Inspect mechanical equipment

E

Check connections

Measurement of insulation resistance

F

Check mechanical operation

NOTE: Check tripping by MN/MX twice a year

Replace MN/MX trip releases

G

Check trip units and electrical auxiliaries

NOTE: Check tripping by VigiPacT Add-on at regular intervals:
  • Every three months in case of absence of local regulation.

  • Once a month for devices in corrosive, dusty, or harsh environment.

Check current transformer module cable connections to the metering device. Check jumpers if metering device is not connected.

Check the characteristics of the trip unit by primary injection

I

Check communication

Check the closing time, opening time and voltage release characteristics

J

Clean equipment

For detailed definition of the maintenance operations, contact Schneider Electric Services.

Maintenance Following Short-Circuit Trip

Test a circuit breaker in severe conditions, in accordance with standard IEC/EN 60947-2, to check that it can break a short-circuit current at maximum permissible value three times.

After a short-circuit fault, it is necessary to:

  • Carefully clean off any traces of black smoke. The smoke particles can conduct electricity.

  • Check the power connections and control wires.

  • Operate the circuit breaker at least five times at zero load.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.