DOCA0187EN-03

Rotary Handle and Accessories Installation Demonstration Video

The following information is available in a demonstration video:

  • Installation of a direct mounted rotary handle and accessories (for example, keylocks) on a ComPacT NSX100–250 circuit breaker

  • Installation of an extended rotary handle and accessories on a ComPacT NSX100–250 circuit breaker

To access the video, click the following link: https://youtu.be/h7ETxmroxiI, copy and paste the link to your Web browser, or scan the QR code.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?