DOCA0187EN-03

Insulated NSX Cord

DANGER
hazard of electric shock, explosion or arc flash
  • It is forbidden to use the insulated NSX cord LV434204 if the system voltage is greater than 690 Vac or 690 Vdc.
  • It is mandatory to use the insulated NSX cord LV434204 if the system voltage is greater than 480 Vac or 480 Vdc, and less than or equal to 690 Vac or 690 Vdc,
Failure to follow these instructions will result in death or serious injury.

Introduction

For system voltages greater than 480 Vac or 480 Vdc, and less than or equal to 690 Vac or 690 Vdc, an insulated variant of the NSX cord must be used, terminated by an electronic module with an RJ45 socket connector. A ULP cord must be used to connect the insulated NSX cord electronic module to a ULP module.

The commercial reference for the insulated NSX cord is LV434204.

The insulated NSX cord electronic module must be supplied with 24 Vdc.

NOTE: The insulated NSX cord cannot be installed in a ComPacT NSX400K circuit breaker.

For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16313AA ComPacT NSX100–630 – Insulated NSX Cord.

Electronic Module Characteristics

The following table summarizes the electronic module characteristics:

Characteristic

Value

Dimensions

27 x 27 x 27 mm

Mounting

On DIN rail

Degree of protection of the installed module

  • On the front panel (wall-mounted enclosure): IP40

  • On the connections (behind the enclosure door): IP20

Operating temperature

-25 to +70 °C

Power supply voltage

24 Vdc -20%/+10% (19.2–26.4 Vdc)

Consumption

  • Typical: 20 mA/24 Vdc at 20 °C

  • Maximum: 30 mA/19.2 Vdc at 60 °C

Insulated NSX Cord Connection

The insulated NSX cord connects to a ULP module:

  • IFM or IFE communication interface

  • FDM121 display

  • IO module

The figure below illustrates an example of connection of ULP modules by using the insulated NSX cord.

A IFM Modbus SL communication interface for one circuit breaker

B RJ45 plug/plug ULP cable

C Insulated ULP module

D Insulated ULP cord

E BSCM Modbus SL/ULP module

F Connector for ComPacT NSX circuit breaker internal connection

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?