DOCA0187EN-03

MA Magnetic Trip Unit

Introduction

The MA trip unit has a high magnetic pickup. It is designed to provide motor-feeders with short-circuit protection.

The MA trip unit can be used to create a type 1 or type 2 coordination motor-feeder.

Description

The adjustment dial is on the front of the trip unit:

A MA magnetic trip unit rating

B Adjustment dial for the magnetic protection pickup Ii

Setting the Magnetic Protection

The magnetic protection pickup Ii is set by:

  • A 9-setting dial for 2.5 A to 50 A ratings

  • A 6-setting dial for 100 A to 220 A ratings

Turning the magnetic protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pickup Ii (in amperes) for magnetic protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ii:

Trip unit rating In (A)

2.5

6.3

12.5

25

50

100

150

220

Pickup Ii (A) +/- 20%

15

38

75

150

300

18

44

88

175

350

20

50

100

200

400

23

57

113

225

450

900

1350

1980

25

63

125

250

500

1000

1500

2200

28

69

138

275

550

1100

1650

2420

30

76

150

300

600

1200

1800

2640

33

82

163

325

650

1300

1950

2860

35

88

175

350

700

1400

2100

3080

Example of Application

Protection of a motor-feeder with the following characteristics:

  • Power supplied by a 1,250 kVA transformer - 400 V, 4%

  • Protection of a motor application defined by:

    • 3-component motor-feeder (circuit breaker, thermal relay, contactor)

    • Direct-on-line starting

    • Motor power 110 kW, that is, In = 196 A

    • Type 2 coordination

The following illustration shows the installation diagram:

1022

Calculations performed on the installation in accordance with the regulations can be used to determine the characteristics of the appropriate ComPacT NSX circuit breaker to install (calculations performed using the Ecostruxure Power Design – Ecodial software).

The following table presents the circuit breaker selection:

Installation

Chosen ComPacT NSX

Comments

In = 196 A

ComPacT NSX250 MA 220

Determination of case size

Isc = 28.5 kA

F

Icu performance can be read from rating plate

Ikmin = 14.8 kA

The following table shows the trip unit protection settings:

Installation

Chosen trip unit

Comments

Ikmin = 14.8 kA

Transient current = 14 In, that is, 2,800 A

Ii = 2,860 A

The Isd protection setting is compatible with:

  • Transient startup currents

  • Short-circuit protection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.