DOCA0187EN-03

MicroLogic 1.3 M Electronic Trip Unit

Introduction

The MicroLogic 1.3 M electronic trip unit with high short-time protection pickup provides motor-feeders with short-circuit protection. Two ratings are available, 320 A and 500 A.

Use the MicroLogic 1.3 M electronic trip unit to create a type 1 or type 2 coordination motor-feeder.

Description

The adjustment dial and indication are on the front face.

A MicroLogic trip unit rating

B Adjustment dial for the short-time protection pickup Isd

C Instantaneous protection pickup Ii

D Test port

E Ready LED (green)

Setting the Short-Time Protection

Set the short-time protection pickup Isd using a 9-setting dial.

Turning the pickup Isd adjustment dial modifies the curves as shown.

The following table shows the values of the pickup Isd (in amperes) for short-time protection (values indicated on the dial) relative to the position of the Isd dial and the values of the pickup Ii for instantaneous protection.

Trip unit rating In

Pickup Isd (A)

Pickup Ii (A)

320 A

1600

1920

2240

2560

2880

3200

3520

3840

4160

4800

500 A

2500

3000

3500

4000

4500

5000

5500

6000

6500

6500

The precision range is +/- 15%.

Example of Application

The following is an example of a motor-feeder application:

  • Power supplied by a 1,250 kVA transformer, 400 V, 4%

  • Downstream power supply of a motor-feeder with the following characteristics:

    • 3-component motor-feeder (circuit breaker, thermal relay, contactor)

    • Direct-on-line starting

    • Motor power 160 kW (In = 280 A)

    • Type 2 coordination

Installation diagram:

Use calculations performed on the installation in accordance with the regulations to determine the characteristics of the appropriate ComPacT NSX circuit breakers to install (calculations performed using the Ecostruxure Power Design – Ecodial software).

Circuit breaker selection

Installation

Circuit breaker

Comments

In = 280 A

ComPacT NSX400 with MicroLogic 1.3 M 320

Motor circuit breaker, case size

Isc = 28.5 kA

F

Read the Icu performance from faceplate label

Ik min = 18.3 kA

Trip unit protection

Installation

Trip unit setting

Comments

Ik min = 18.3 kA

Inrush current = 14 In

Isd = 4,160 A

The Isd protection setting is compatible with:

  • Transient startup currents

  • Short-circuit protection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.