EIO0000004266.03

Attaching USB Clamp mini-B

When using the USB micro-B cable (option), you can use the USB mini-B clamp (sold separately) to prevent the cable from being disconnected.

DANGER
EXPLOSION HAZARD
  • Confirm that the USB cable has been fixed with the USB clamp before using the USB interface.
  • Remove power before attaching or detaching any connectors to or from this product.
  • Use the USB (micro-B) interface for temporary connection only during maintenance and setup of the device.
  • Do not use the USB interface in hazardous locations.
Failure to follow these instructions will result in death or serious injury.
  1. Insert the USB cable into the USB (micro-B) interface.
    1. USB interface

  2. Attach the USB clamp to fix the USB cable in place. Insert the USB holder into the USB (micro-B) interface.

      B.  USB clamp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.