EIO0000004266.03

Touch Panel

Touch panel type Resistive film (analog)
Touch points Single touch
Touch panel resolution 1,024 x 1,024
Touch panel service life 1 million times or more

The touch panel does not support multi-touch (two-point touch/multiple-point touch). If you touch multiple points on the touch panel, it may operate as if you touched the center-point of the multiple touches. For example, if you touch two or more points on the touch panel and at the center of the touches is a switch for a drive system, even though you did not directly touch that switch, it may function as if you did.

WARNING
UNINTENDED EQUIPMENT OPERATION
Do not touch two or more points on the touch panel.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.