EIO0000004266.03

Parts Identification

HMIET6400 and HMIET6500

NOTE: The figures below show HMIET6500.
Front
Rear
Top
Bottom
  1. Status LED

  2. USB (Type-A) interface

  3. USB (micro-B) interface

  4. Battery slot

  5. Ethernet interface

  6. Serial interface (COM2)

  7. Serial interface (COM1)

  8. Power connector

*1 This mark indicates the safety messages about the power wiring. Refer to Wiring the Power Supply.

*2 This mark identifies the safety messages about the battery. Refer to Replacing the Battery.


HMIET6401 and HMIET6501

NOTE: The figures below show HMIET6501.
Front
Rear
Top
Bottom

 A.  Status LED

 C.  USB (micro-B) interface

 D.  Battery slot

 F.  Serial interface (COM2)

 G.  Serial interface (COM1)

 H.  Power connector

*1 This mark indicates the safety messages about the power wiring. Refer to Wiring the Power Supply.

*2 This mark identifies the safety messages about the battery. Refer to Replacing the Battery.


HMIET6600 and HMIET6700

NOTE: The figures below show HMIET6600.
Front
Rear
Bottom
  1. Status LED

  2. USB (Type-A) interface

  3. USB (micro-B) interface

  4. Battery slot

  5. Ethernet interface

  6. Serial interface (COM2)

  7. Serial interface (COM1)

  8. Power connector

*1 This mark indicates the safety messages about the power wiring. Refer to Wiring the Power Supply.

*2 This mark identifies the safety messages about the battery. Refer to Replacing the Battery.

NOTE: HMIET6700 Ethernet 2 interface (ETH2) is not available. Do not remove the RJ-45 port blocker.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.