EIO0000004266.03

LED Indications

Status LED

After the power is turned on, the normal status indication by the LED is: red light > blinking orange > green light.

Color Indicator HMI operation
Green ON In operation/offline
Orange

ON

Software starting up
Red ON Power is ON.
- OFF Power is OFF.

For other LED indications, refer to the manual of your screen editing software.

Ethernet LED

Color Indicator Description
Green (Link) ON Data transmission is available.
OFF No connection or error
Green (Active) Flashing Data transmission is occurring.
OFF No data transmission
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.