EIO0000004266.03

Clock

RTC accuracy

Deviation of ±60 seconds per month (at 25 °C [77 °F] and power is OFF).

Clock data backup

Lithium metal battery (primary battery, replaceable)
Battery life: 5 years (approximate)

Variations in operating conditions and battery life can cause clock deviations from -380 to +90 seconds per month. If you use this product in a system where timing is critical, adjust the clock at regular intervals.

If the battery is depleted or removed, the clock data will be lost. To replace the battery, refer to Replacing the Battery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.