EIO0000004266.03

Serial Interface

The serial interface is not isolated. The SG (signal ground) and FG (frame ground) terminals are separated inside this product.

DANGER
ELECTRIC SHOCK
  • Make a direct connection between the frame ground (FG) terminal and ground.
  • Do not connect other devices to ground through the frame ground (FG) terminal of this device.
  • Install all cables according to local codes and requirements. If local codes do not require grounding, follow a reliable guide such as the US National Electrical Code, Article 800.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a D-Sub 9 pin connector that has jack screws.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

Serial Interface COM1 RS-232C

D-Sub 9 pin plug connector

Product side:

Pin No. RS-232C
Signal name Direction Description
1 CD Input Carrier Detect
2 RD (RXD) Input Receive Data
3 SD (TXD) Output Send Data
4 ER (DTR) Output Data Terminal Ready
5 SG - Signal Ground
6 DR (DSR) Input Data Set Ready
7 RS (RTS) Output Request To Send
8 CS (CTS) Input Clear To Send
9 NC - No connection
Shell FG - Frame Ground
Recommended jack screw is #4-40 (UNC).

Serial Interface COM2 RS-422/485

D-Sub 9 pin plug connector

Product side:

Pin No. RS-422/RS-485
Signal name Direction Description
1 RDA Input Receive Data A (+)
2 RDB Input Receive Data B (-)
3 SDA Output Send Data A (+)
4 NC - No connection
5 SG - Signal Ground
6 NC - No connection
7 SDB Output Send Data B (-)
8 NC - No connection
9 NC - No connection
Shell FG - Frame Ground
Recommended jack screw is #4-40 (UNC).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.