EIO0000004266.03

Installation Procedure

This section describes how to install this product to the panel.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE
  • Always use the installation gasket.
  • Keep this product stabilized in the panel cutout while you are installing or removing the screw fasteners.
  • Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Place this product on a clean and level surface with the screen facing down.
  2. Check that the gasket is seated securely into the bezel groove, which runs around the perimeter of the display panel frame.
    NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water.
  3. Based on this product's Panel Cutout Dimensions, open a mount-hole on the panel and attach this product to the panel from the front side.
    NOTE: This product has a hook at the top to prevent it from falling. Insert the bottom part of the product into the panel opening, and then insert the top part while pushing the hook down.
    1. Hook

  4. Insert the installation fasteners into the panel‘s insertion slots of this product.
    1. Insertion slots

    2. Insertion slots (except for the HMIET6400/HMIET6401)

    3. Panel

    4. Installation fastener for HMIET6400/HMIET6401, HMIET6500/HMIET6501 and HMIET6600

    5. Installation fastener for HMIET6700

    The number of installation fasteners for each model is as follows.

    HMIET6400/HMIET6401 Top - 2, Bottom - 2
    HMIET6500/HMIET6501, HMIET6600 and HMIET6700 Top - 2, Bottom - 2, Left - 1, Right - 1
  5. Tighten the installation fastener’s screws with a screwdriver.
    NOTE:
    • The necessary torque is 0.5 N•m (4.4 lb-in).

    • The installation fasteners for HMIET6700 can be screwed by hand too.

    • If the fasteners are not correctly attached, the panel may shift or fall out.

    1. Screwdriver

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.