EIO0000004266.03

Package Contents

Verify all items listed here are present in your package.

If you find anything damaged or missing, please contact customer support immediately.

WARNING
UNINTENDED EQUIPMENT OPERATION
Do not use damaged products or accessories.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Easy Harmony ET6 x 1

  2. Installation gasket (attached to this product) x 1

  3. DC power connector x 1

  4. (D-1)

    • Installation fasteners x 4 (for HMIET6400/HMIET6401)

    • Installation fasteners x 6 (for HMIET6500/HMIET6501 and HMIET6600)

    (D-2)

    • Installation fasteners x 6 (for HMIET6700)

  5. Instruction sheet x 1

Revision and QR Code

You can identify the product version (PV), revision level (RL), and the software version (SV) from the product label.

NOTE: Depending on the model, the product label may not be marked RL.

You can also check the contents of this manual by using the QR code on the product label. Confirm the location of the QR code below and refer to the manual.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.