EIO0000004266.03

Accessories

This section introduces optional items that are sold separately.

Products may change or be discontinued without notice. Please check our website for the latest information.
www.se.com/docs

For host controllers and connection cables, refer to the corresponding device driver manual of your screen editing software.

Product name Product number Description
USB (micro-B) interface
USB Transfer Cable HMIZG936 Cable for transferring screen data from a PC (USB Type-A) to this product (USB micro-B)
USB (micro-B) Front Cable HMIZSUSBB2 Extension cable that attaches USB interface to front panel.
USB Clamp Type mini B*1 HMIZSCLP3 Clamp to prevent disconnection of USB cable (for 1 port, USB Type mini B, 5 pieces/set)
USB (Type-A) interface
USB Front Cable (1 m) XBTZGUSB Extension cable that attaches USB interface to front panel.

USB Clamp Type-A (1 port)

HMIZGCLP1 Clamp to prevent disconnection of USB cable (for 1 port, USB Type-A, 5 pieces/set)
Others
Screen Protection Sheet HMIZD66W Disposable, dirt-resistant sheet for the display for 12-inch Wide screen (5 sheets/set).
UV Protection Sheet HMIZUV6W Sheet to protect the display from dirt and ultraviolet light, for 12-inch Wide screen (1 sheet).
Screen Protection Sheet with UV Protected HMIZG63W Disposable, dirt-resistant and ultraviolet protection sheet for 7-inch Wide screen (1 sheet/set).
HMIZG65W1 Disposable, dirt-resistant and ultraviolet protection sheet for 10-inch Wide screen (1 sheet/set).
HMIZG67W Disposable, dirt-resistant and ultraviolet protection sheet for 15-inch Wide screen (1 sheet/set).

*1 USB Clamp mini-B can be used for optional USB micro-B cables.

Maintenance Accessories

Product name Product number Description
Installation Fastener HMIZGFIX3 Used to install 7-inch, 10-inch and 12-inch Wide model into a solid panel (4 pieces/set).
HMIZSFIXTF1 Used to install 15-inch Wide model into a solid panel (2 pieces/set).
DC Power Supply Connector XBTZGPWS1 Connector for a DC power supply cable.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.