EIO0000004266.03

Precautions for Building into an End-use Product

This product is designed for use on flat surfaces of enclosures.
For HMIET6400, HMIET6401, HMIET6500, HMIET6501 and HMIET6600, the front surface is rated for IP65 enclosure.
For HMIET6700, the front surface is rated for IP65 and Type 4X (indoor use only) enclosure.

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product’s overall enclosure.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate this product with its front panel facing outward.

NOTE: IP65 is not part of the UL certification.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.