Product Related Information
If the equipment is used in a manner not specified by the manufacturer, the protection provided by the equipment may be impaired.
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION,
OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
EXPLOSION HAZARD
Failure to follow these instructions will result in death or serious injury.
|
Critical alarm indicators and system functions require independent and redundant protection hardware and/or mechanical interlocks.
When you cycle power, wait at least 10 seconds after it has been turned off. If this product is restarted too quickly, it may not operate correctly.
In the event the screen cannot be properly read, for example, if the backlight is not functioning, it may be difficult or impossible to identify a function. Functions that may present a hazard if not immediately executed, such as a fuel shut-off, must be provided independently of this product. The machine’s control system design must take into account the possibility of the backlight no longer functioning and the operator being unable to control the machine or making mistakes in the control of the machine.
![]() |
---|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control" and to NEMA ICS 7.1 (latest edition), "Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems" or their equivalent governing your particular location.
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The following characteristics are specific to the LCD panel and are considered normal behavior:
-
LCD screen may show unevenness in the brightness of certain images or may appear different when seen from outside the specified viewing angle. Extended shadows, or crosstalk may also appear on the sides of screen images.
-
LCD screen pixels may contain black and white colored spots and color display may seem to have changed.
-
When experiencing vibrations within a certain frequency range and vibration acceleration is above what is acceptable, the LCD screen may partially turn white. Once the vibration condition ends, the whitening of the screen is resolved.
-
When the same image is displayed on the screen for a long period, an afterimage may appear when the image is changed.
-
The panel brightness may decrease when used for a long time in an environment continuously filled with inert gas. To prevent deterioration of panel brightness, regularly ventilate the panel. For more information, please contact your local distributor.
www.se.com
![]() |
---|
SERIOUS EYE AND SKIN INJURY
The liquid in the LCD panel contains an irritant:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Cybersecurity Best Practices
To help keep your Schneider Electric products secure and protected, we recommend that you implement
the cybersecurity best practices. Following the recommendations may
help significantly reduce your company’s cybersecurity risk.
For the recommendations, refer to the following URL:
https://www.se.com/en/download/document/7EN52-0390/