DOCA0297EN-02

Go2SE Landing Page

Presentation

When the QR code on the front face of a TS trip system is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed.

The landing page displays:

  • Information about the TS trip system.

  • A list of menus.

Landing Page Description

The landing page is accessible from Android and iOS smartphones. It displays the same list of menus with slight differences in presentation.

The following example shows the landing page displayed on an Android smartphone:

  1. TS trip system commercial reference

    .
  2. TS trip system description

    .
  3. TS trip system serial number

    .
  4. Landing page menus. See the following menu descriptions for details.

  5. Downloadable applications.

Characteristics

Selecting this menu gives access to a product datasheet with detailed information about the TS trip system.

Documentation

Selecting this menu gives access to the technical publications of:

  • TS trip systems

  • EasyPact MVS devices

mySchneider App

Selecting this application gives access to the Schneider Electric customer care mobile application mySchneider app that can be downloaded on Android and iOS smartphones. For smartphone compatibility, check on your application store. The customer care application offers self-service instructions and easy access to expert support and information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?