Fixed Device
Fixed Device Description
The following image shows the standard version of the fixed device (no optional accessories).
Fixed Device Accessories Description
The following image shows the accessories available for the fixed device.
The following images zoom in on the accessories for the fixed device:
Fixed Device Terminal Block Description
Assignment of Terminal Blocks
DANGER |
|---|
|
HAZARD OF ELECTROCUTION FOR VOLTAGES ABOVE 480 VaC
If voltage greater than 480 Vac is connected to a terminal,
it is forbidden to connect adjacent terminals to a 24 Vdc SELV (Safety
Extra Low Voltage) power supply in order to observe the insulation
distances.
Failure to follow these instructions will result in death or serious injury.
|
The following table describes the assignment and the availability of the terminal blocks for fixed devices:
-
Standard terminal blocks and the associated accessories are delivered with the device.
-
Optional terminal blocks are delivered with the device only if the associated optional accessories are installed in the device.
-
N/A indicates that the terminal blocks and the associated optional accessories are not compatible with the device.
|
Marking |
Description |
Device |
|---|---|---|
|
COM |
Not used |
Not used |
|
UC1 |
Not used |
Not used |
|
UC2 |
Neutral external sensor |
Standard on devices with TS 6.0S trip system Not used on devices with TS 2.0, 5.0, 2.0S, or 5.0S trip system |
|
UC3 |
Not used |
Not used |
|
SDE2/RES |
Not used |
Not used |
|
M2C/UC4 |
Not used |
Not used |
|
SDE1 |
SDE1 fault-trip indication contact |
Standard |
|
MN/MX2 |
MN undervoltage release or MX2 opening voltage release |
Optional |
|
MX1 |
MX1 opening voltage release |
Standard |
|
XF |
XF closing voltage release |
Standard |
|
PF |
PF ready-to-close contact |
Optional |
|
MCH |
MCH gear motor |
Standard |
|
OF1-OF4 |
4 OF indication contacts |
Standard |
DANGER