DOCA0297EN-02

Resetting the Device

Resetting Conditions

After a trip, the device must be reset before closing it.

Resetting the Device

The device can be reset in different ways, according to the device configuration and its accessories:

Type of resetting

Accessories

Resetting action

Mechanical with the blue fault-trip reset button

Push in the blue fault-trip reset button on the front of the device. This resetting action is always possible. Pushing in the blue fault-trip reset button resets the SDE fault-trip indication contact, and allows the device to be closed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?