EasyPact MVS1 Range
The EasyPact MVS1 range is made of:
-
Circuit breakers with TS Trip System and switch-disconnectors, described in this guide.
-
Circuit breakers with ET, ETA and ETV Trip Systems, described in MVS21734 EasyPact MVS IEC Circuit Breakers with ET, ETA and ETV Trip System From 630 to 4000 A – User Guide.
Convention
This guide applies to EasyPact MVS1 circuit breakers and switch-disconnectors.
EasyPact MVS1 Circuit Breakers with TS Trip Systems
The range of EasyPact MVS1 circuit breakers with TS trip system offers current ratings from 630 to 1600 A, for AC power systems up to 440 Vac. The range is covered by one frame size.
EasyPact MVS1 circuit breakers with TS trip system are available:
-
In the following power systems:
-
3-pole (3P)
-
4-pole (4P)
-
-
In the following installation types:
-
Fixed-mounted devices
-
Drawout devices
-
For information about TS trip system, refer to DOCA0299●● EasyPact MVS - TS Trip System - User Guide.
EasyPact MVS1 Circuit Breakers Performances
EasyPact MVS1 circuit breakers with TS trip system are available with the following performance level:
- C: high short-circuit level (66 kA) with high selectivity (50 kA) network
EasyPact MVS1 Switch-Disconnector Performances
The switch-disconnector functions in the CA performance level (Icw = 50 kA/1s).
Neutral Position on 4P Devices
On 4P devices, the neutral is on the left side as standard. A right side neutral version is not available for circuit breakers.