Locking the Device in Open Position with Keylocks
Description
Optional keylocks can be used:
-
To lock one EasyPact MVS1 device in the open position. When locked the device cannot be closed either locally with the closing pushbutton or remotely.
-
To interlock several EasyPact MVS1 device locked with the same key.
To use keylocks to lock the device in the open position, an optional OFF-position locking accessory is necessary.
VSPO OFF-Position Locking Accessory
The OFF-position locking accessory is an optional accessory
that is mounted on the front of the device.
The OFF-position keylocking accessory can be fitted with one Profalux keylock.
For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: MVS21736.
Locking the Device in the Open Position
For devices equipped with two keylocks, locking with one key is sufficient to lock the device in the open position.