DOCA0297EN-02

Drawout Device

Definition

A drawout device is composed of the moving part (also called the device) and the fixed part (or chassis).

Drawout Device Moving Part Description

The following image shows the standard version of the moving part of a drawout device (no optional accessories).

A Carrying handle

B Arc chute

C Blue fault-trip reset button

D Opening pushbutton

E Closing pushbutton

F Disconnectable contact block cover

G Front cover

H Spring charging handle

I VBP pushbutton locking cover (optional)

J Rating plate

K Spring charged and ready-to-close indicator

L Main-contact position indicator

M Window to consult the optional CDM mechanical operation counter

N Trip system

O Product identification label, with manufacturing label

Drawout Device Accessories Description

The following image shows the accessories available for the moving part of a drawout device.

A VDC mismatch protection (optional)

B Disconnectable contact block

C Four OF indication contacts (standard)

D MCH gear motor (standard)

E CDM mechanical operation counter (optional)

Z1, Z2 See following images

The following images zoom in on the accessories for the moving part of a drawout device.

F Standard SDE1 fault-trip indication contact

G MN undervoltage release or MX2 opening voltage release (optional)

H XF closing voltage release (standard)

I MX1 opening voltage release (standard)

J PF ready-to-close contact (optional)

K VSPO OFF-position locking by keylocks (optional)

Chassis Description

The following image shows the standard version of the chassis (no optional accessories).

A Carrying grip

B Terminal blocks for standard accessories

C Terminal block identification plate

D Chassis locking by padlocks

E Position indicator

F Racking handle socket

G Position release button

H Racking handle storage space

I Racking handle

J Drawout grip

K Extension rail

L Top safety shutter

M Product identification label with manufacturing date

N Bottom safety shutter

Chassis Accessories Description

The following image shows the accessories available for the chassis.

A VDC mismatch protection

B Terminal blocks for optional accessories

C VSPD chassis locking by keylocks

D VPOC open-door racking interlock

E Device auxiliary terminal shield

F VPEC door interlock

Chassis Terminal Block Description

Terminal block supplied as standard on the chassis

Terminal block supplied as standard with 3P chassis only

Terminal block for optional accessories on the chassis

Terminal block not used on the chassis

Assignment of Chassis Terminal Blocks

DANGER
HAZARD OF ELECTROCUTION FOR VOLTAGES ABOVE 480 VaC
If voltage greater than 480 Vac is connected to a terminal, it is forbidden to connect adjacent terminals to a 24 Vdc SELV (Safety Extra Low Voltage) power supply in order to observe the insulation distances.
Failure to follow these instructions will result in death or serious injury.

The following table describes the assignment and the availability of the terminal blocks for drawout devices:

  • Standard terminal blocks are delivered on the chassis, even if the associated accessories are not installed in the devices.

  • Optional terminal blocks are delivered on the chassis only if the associated optional accessories are installed in the devices.

  • N/A indicates that the terminal blocks and the associated optional accessories are not compatible with the devices.

Block

Marking

Description

Device

A

CD1-CD2

2 CD disconnected position contacts

Optional

B

COM

Not used

Not used

UC1

Not used

Not used

UC2

Neutral external sensor

Standard on 3P devices

Optional on 4P devices

UC3

Not used

Not used

SDE2/RES

Not used

Not used

M2C/UC4

Not used

Not used

SDE1

SDE1 fault-trip indication contact

Standard

MN/MX2

MN undervoltage release

or MX2 opening voltage release

Optional

MX1

MX1 opening voltage release

Standard

XF

XF closing voltage release

Standard

PF

PF ready-to-close contact

Optional

MCH

MCH gear motor

Standard

OF1-OF4

4 OF indication contacts

Standard

C

CE1–CE3

3 CE connected position contact

Optional

CT1

1 CT test position contact

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?