DOCA0297EN-02

Diagnosing Alarms

Diagnosis Procedure

The following table shows the sequence of actions to take after an alarm is detected by the TS trip system. Further explanation of each action is given in the following paragraphs.

Step

Action

1

Identify the alarm detected.

2

Consult the active alarms by using:

  • a smartphone with EcoStruxure Power Device app connected to the TS trip system through NFC wireless communication

    .
  • a PC with EcoStruxure Power Commission software connected to the TS trip system: through USB connection.

3

Perform the recommended actions described in DOCA0299●● EasyPact MVS - TS Trip System - User Guide.

4

Press the button for 3 seconds to reset the latched events and switch off the trip cause LEDs and the status bar.

Identifying the Alarm Detected

The TS trip system indicates alarms with:

  • The status bar is on red for high-severity detected alarms

  • The status bar is on orange for medium-severity detected alarms

Description

Indication LEDs

Major or minor internal malfunction detected, corrective action to be planned.

Ready LED: blinking green

Status bar: orange on

Service LED: red on

All trip cause LEDs: off

Overload pre-alarm: 90% Ir < Phase current < 105% Ir

Ready LED: blinking green

Status bar: orange on

Service LED: off

L trip cause LED: red on

Other trip cause LEDs: off

Ground fault alarm: Ig current ≥ 80 % Ig

Ready LED: blinking green

Status bar: orange on

Service LED: off

G trip cause LED: red on

Other trip cause LEDs: off

Overload alarm: current ≥ 105 % Ir

Ready LED: blinking green

Status bar: red on

Service LED: off

L trip cause LED: red on

Other trip cause LEDs: off

For more information, refer to the event messages in DOCA0299●● EasyPact MVS - TS Trip System - User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?