DOCA0297EN-02

Closing the Device

Closing Conditions

To close the device, the following conditions must be met:

  • Device is open (O).

  • Closing spring is charged.

  • The device is ready to close, OK is displayed.

NOTE: An opening order always takes priority over a closing order. The device cannot be closed while an opening order is being received. If OK is crossed-out on the ready-to-close indicator, an order to open is being received (either electrically or mechanically) and must be ended before OK can be displayed.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not re-close the device on an electrical fault. First inspect and, if necessary, repair the downstream equipment.
Failure to follow these instructions will result in death or serious injury.

Closing the Device

The following tables present the different ways to close the device.

Closing type

Accessories

Closing action

Mechanical

Press the closing pushbutton on the front of the device.

The closing action is possible when the closing conditions are met.

External pushbutton

  • External pushbutton wired by customer

  • XF standard closing voltage release

  • MCH gear motor

Press the external pushbutton, which is connected to the XF closing voltage release through the customer terminal block.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?