DOCA0297EN-02

Locking the Safety Shutters

Description

A shutter lock locks the safety shutter in closed position so that a drawout EasyPact MVS1 device cannot be connected in its chassis.

The top and bottom safety shutters can be locked independently.

Locking the Safety Shutters

Place two padlocks on the top and bottom shutter locking guides to lock the shutters.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: MVS21737.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?