DOCA0297EN-02

Device Identification

Identification

The EasyPact MVS1 device can be identified in the following ways:

  • Rating plate on the device

  • QR code located on the front face of the trip system of the device

  • Identification labels on the device and on the chassis

A Product identification label

B Accessory voltages label

C QR code to access product information

D Rating plate

Product Identification Label

Legend

Description

Explanation

A

Product code

The product code is a line of code representing the complete configuration of a EasyPact device. It is automatically generated for each EasyPact device after completing the configuration by using the Product Selector configuration tool.

The product code appears on the invoice and on the delivery documents as well as on the EasyPact device and packaging labels.

The product code can be entered in the Product Selector configuration tool, which generates the complete configuration of the EasyPact device.

B

Schneider Electric internal identification numbers

C

Item number/quantity

Item number/quantity is printed on the label. Only the useful character is printed.

D

Datamatrix

Datamatrix contains the serial number of the EasyPact device.

E

Manufacturing country

Country where the EasyPact device is manufactured.

F

Device serial number

The device serial number is coded PPYYWWDNNNN, where:

  • PP: Plant code

  • YY: Year of manufacture

  • WW: Week of manufacture

  • D: Day of the week of manufacture (Monday = 1)

  • NNNN: The production number of the device on the day. Ranges from 0001 to 9999.

For example, PP240820001 is the first device manufactured at plant PP on Tuesday, February 20, 2024.

G

Description of device

The description of the device, specifies the following characteristics:

  • Range

  • Performance level

  • Rating

  • Number of poles

  • Trip system type

Accessory Voltages Label

The accessory voltages label gives the voltage of the accessories which are installed in the device and which need to be connected to a power supply.

Rating Plate

The rating plate with the device information is located on the front cover of the device.

A Device size and rated current x 100 A

B Ui: rated insulation voltage

C Uimp: rated impulse withstand voltage

D Ue: rated operational voltage

E Ics: rated service breaking capacity

F Selectivity category as per IEC 60947-2

G Type of device: circuit breaker or switch-disconnector, suitable for insulation

H Icu: rated ultimate short-circuit breaking capacity

I Icw: rated short-circuit breaking capacity

J Frequency

QR Code

When the QR code on the front face of a TS trip system is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE Landing Page is displayed.

The landing page displays:

  • Information about the TS trip system.

  • A list of menus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?