Troubleshooting: Mechanical Control Operations
Definition
Mechanical control operations are operations that are made using the opening or closing pushbuttons.
Circuit Breaker Cannot be Closed by Using the Mechanical Closing pushbutton
|
Symptom |
Probable causes |
Solutions |
|---|---|---|
|
The blue fault-trip reset button is popped out. |
The blue fault-trip reset button has not been reset. |
|
|
- |
Circuit breaker is padlocked or keylocked in the open position. |
Unlock the circuit breaker. |
|
- |
Circuit breaker is interlocked mechanically in a mechanical interlocking system. |
|
|
The closing spring and ready-to-close indicator shows that the mechanism is discharged. |
Stored energy mechanism is not charged. |
|
|
The closing spring and ready-to-close indicator shows that the mechanism is charged but the circuit breaker is not ready to close. |
MX opening voltage release is permanently powered. |
As there is an opening order, determine the origin of the order. The order must be canceled before the circuit breaker can be closed. |
|
MN undervoltage release is not powered due to an opening order. |
As there is an opening order, determine the origin of the order. The order must be canceled before the circuit breaker can be closed. |
|
|
MN undervoltage release is not powered due to insufficient voltage power supply. |
Check the voltage and the MN supply circuit (V > 0.85 Un). If the problem persists, replace the MN undervoltage release. |
|
|
The position release button on the chassis of the drawout circuit breaker is pushed in. |
Circuit breaker is not correctly connected. |
Terminate racking in (connection) of the circuit breaker, making sure that it is fully inserted in the chassis, to the connected position. Check that the position release button is popped out. |
Circuit Breaker Cannot be Opened by Using the Mechanical Opening pushbutton
|
Probable causes |
Solutions |
|---|---|
|
Operating mechanism incident or welded contacts. |
Contact your field service representative. |