Mechanical Interlocking for Transfer Switches
Description
The mechanical interlocking for transfer switches between EasyPact MVS1 devices prevents the interlocked devices from closing at the same time.
VBP Pushbutton Locking Accessory
The VBP pushbutton locking accessory provides redundancy in addition to the mechanical interlocking system.
The use of the pushbutton locking cover is mandatory on each interlocked EasyPact MVS1 device. The closing pushbuttons of the interlocked devices must be locked by padlocks sharing one key to help avoid simultaneous closing orders of interlocked devices.
For more information about the pushbutton locking cover, refer to VBP Pushbutton Locking Accessory.
Mechanical Interlocking Between Two Devices
For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: MVS21738.
IVE Electrical Interlocking Unit
Electrical interlocking between EasyPact MVS1 devices can be done using the IVE electrical interlocking unit or by using dedicated wiring. The IVE unit is suitable for two devices only. For three devices, dedicated wiring is required to perform the electrical interlocking.
For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: 51201201AA.