DOCA0297EN-02

Final Checks and Reporting

Final Checks

After completing the commissioning tests, check the following:

Step

Action

1

Check that connections are made with the correct tightening torque, that there are no tools or objects inside the equipment, and that all circuit breakers, doors, and protective covers are in position.

2

Check that the circuit breaker is off (open position) and the closing spring is charged.

Project Report Generated by EcoStruxure Power Commission Software

EcoStruxure Power Commission software generates a project report with a list of the circuit breakers for that project. For each EasyPact MVS circuit breaker it provides the following information:

  • The circuit breaker identification data

  • The TS identification data

  • The protection settings for the TS trip system

  • The alarm settings

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?