DOCA0299EN-03

Event History

Overview

All events are logged in one of the histories of the TS trip system:

  • Trip

  • Protection

  • Diagnostic

All severities of events are logged, including low-severity events.

Events logged in histories are displayed with:

  • EcoStruxure Power Device app

  • EcoStruxure Power Commission software

Events logged in histories can be erased with EcoStruxure Power Commission software.

The following information is logged in a history for each event:

  • Event ID: event code

  • Event type: Entry/Exit or Pulse

  • Context data (only for certain events)

Maximum Number of Events in Each History

Each history has a predefined maximum size. When a history is full, each new event overwrites the oldest event in the relevant history.

Event history

Maximum number of events stored

TS 2.0 and 5.0 history

TS 2.0S, 5.0S, and 6.0S history

Trip

1

30

Protection

0

25

Diagnostic

0

35

Displaying Event History on EcoStruxure Power Commission Software

All events logged in histories can be consulted using EcoStruxure Power Commission software. The events can be exported as an Excel file.

Events in histories are displayed in chronological order, starting with the most recent event.

Displaying Event History on EcoStruxure Power Device App

The latest five events logged in histories are displayed on the EcoStruxure Power Device app.

Events in histories are displayed in chronological order, starting with the most recent event.

Events can be sorted by sequence number, and filtered by using the following criteria:

  • Type

  • History

Clicking on a specific event in the list displays a list of all occurrences of the same event, in chronological order.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?