DOCA0299EN-03

Event Display

Introduction

The event status table contains the status of all events at the time of consultation. The status can be inactive, active, or held.

Events which are in the active and held state are displayed on the following interfaces:

  • EcoStruxure Power Commission software.

  • EcoStruxure Power Device app.

Displaying Events on EcoStruxure Power Commission Software

All events severity, active and held events are displayed.

Events can be sorted by:

  • Severity:

    • High severity events

    • Medium severity events

    • Low severity events

  • History

  • Type

Displaying Events on EcoStruxure Power Device App

By default, events are sorted chronologically. They can be sorted by other parameters such as severity, type or history.

The EcoStruxure Power Device app displays only a selection of events, see the details in the Event List.

The EPD App displays events on the Alarms screen.

- The Active tab displays up to 5 active trips or alarms from a selection of events. Refer to Event List, to get the list of alarms that can be displayed by EcoStruxure Power Device app.

The details of the active trips is also available... TBC @Ray

- The History tab displays the last non-active trip event with details ... + list of the details given for a trip @Ray

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.