DOCA0299EN-03

USB Connection

Description

From a PC running EcoStruxure Power Commission software, you can access all of the monitoring and test functions of the TS trip system by connecting a PC totrip system through the function test and isolation module.

Prerequisites for Using a USB Connection

The prerequisites for establishing a USB connection are:

  • You must have the USB driver installed on the PC.

  • You must have physical access to the TS trip system to connect the cable directly to the trip system.

  • You must have the function test and isolation module (commercial reference LV910200SP) to connect the USB port of the PC to the TS trip system.

Connecting a PC Running EcoStruxure Power Commission Software to 5-Pin Plug

Follow the procedure below to connect to the TS trip system using the function test and isolation module:

  1. Connect your PC to the TS trip system through the function test and isolation module (same connection as for testing the protection functions).

    The PC provides power to the TS trip system if necessary.

  2. Start EcoStruxure Power Commission software on the PC and log in.

  3. On the EcoStruxure Power Commission home page, connect to the TS trip system. There are different ways to connect EcoStruxure Power Commission software to the TS trip system, depending on whether it is the first connection and how the device is discovered. For more information, refer to EcoStruxure Power Commission Online Help.

  4. With EcoStruxure Power Commission software connected to the TS trip system you have access to all functions of the software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?