DOCA0299EN-03

Circuit Breaker Maintenance Counters

Presentation

The maintenance indicator helps to anticipate the replacement of the breaking block before mechanical or electrical breakdown. Circuit breaker service life depends on the daily number of operating cycles with or without current.

Operating Principle

Each time the circuit breaker operates (performs an open and close cycle with or without current), the corresponding mechanical and electrical operating counters are incremented.

The list of maintenance counters:

  • Counter of total operations

  • Total trip operations

  • Counter of long-time trips

  • Counter of short-time trips

  • Counter of instantaneous trips

  • Counter of ground-fault trips

  • Counter or trips during tests

Data Availability

Data is available with EcoStruxure Power Device app through NFC wireless communication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?