DOCA0299EN-03

Testing the TS Trip System

Test the TS Trip System using EcoStruxure Power Commission software installed on a PC and connected to the TS Trip System through the function test and isolation module.

Testing Architecture

  1. 5-pin cable for TS trip system

  2. Cable with 2 USB-C connectors

For more information, refer to PKR4267807 Function test and isolation module instruction sheet.

Test Functions with EcoStruxure Power Commission Software

EcoStruxure Power Commission software allows you to perform the following actions on a TS trip system communicating through the function test and isolation module:

  • Automatic trip curve tests

  • Device check up (Force trip test)

  • Preparation for primary injection tests

For more information, refer to relevant document:

  • EasyPact MVS1 Circuit Breakers with TS Trip System - User Guide

  • EasyPact MVS2 Circuit Breakers with TS Trip System - User Guide

Trip System Test Mode

The test mode is activated when EcoStruxure Power Commission software is connected to the device through a PC connected to the 5-pin plug on the TS trip system and the Force trip button is clicked. For more information, refer to EcoStruxure Power Commission Online Help.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?