DOCA0299EN-03

Password Management

General Description

Remote access to data on TS trip system by using the EcoStruxure Power Commission software is protected by password.

A TS trip system has a password for administrator profile.

The following table shows the functions allowed for each user profile:

User profile

Read ID

Monitoring

Test

Recovery function

Firmware update

Administrator

Not login

No user mode(1)

(1) The device acts as No user mode if the user creation step is skipped.

The following table describes the functions:

Function

Description

Read ID

Read the identification number of the trip system

Monitoring

Read all settings, measurements, and data

Test

Send test commands

Recovery function

Reset password and delete all users

Firmware update

Update firmware to the latest version

Default Passwords

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The default Administrator password is +Schneider0.

Changing a Password

A password can be changed with EcoStruxure Power Commission software.

Entering the current password for a given user profile is required to change the password of this user profile. Entering the Administrator password enables you to change the password of any user profile.

A password is composed of exactly 8-32 ASCII characters. It is case-sensitive and the allowed characters are:

  • Digits from 0 to 9

  • Letters from a to z

  • Letters from A to Z

  • ASCII code special characters from 33 ("!") to 126 ("~")

Password Reset

In the case that the Administrator password is lost or forgotten, the password can be reset to the default password with EcoStruxure Power Commission software, and with the support of the Schneider Electric Customer Care Center.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.