DOCA0299EN-03

Long-Time Overcurrent Protection (L or ANSI 49RMS/51)

Presentation

Long-time overcurrent protection helps to protect cables, busbars, and busbar trunking against overloads, based on the true RMS current. It is implemented independently for each phase and for the neutral.

This protection function is an overcurrent time-dependent protection with thermal memory. It operates as a thermal image, using the heating and cooling model of a conductor. After tripping, the protection continues to integrate the cooling of the conductor.

This protection function can be used also for transformer or generator protection thanks to the wide range of settings offered.

Availability

Long-time overcurrent protection is available on:

  • TS 2.0 and 2.0S, 5.0 and 5.0S, and 6.0S trip system

  • 3-pole and 4-pole circuit breakers

Long-time overcurrent protection is powered by the current flowing through the internal current transformers of the circuit breaker and it does not require additional external power supply.

Operating Principle

  • Long-time overcurrent protection is based on the true RMS current of phases and neutral.

  • Long-time overcurrent protection is implemented independently for each phase and for neutral when present

    .

Setting the Protection

The long-time overcurrent protection settings are:

  • Ir: long-time overcurrent protection pickup

  • tr: long-time overcurrent protection time delay

They can be set by using the Ir and tr rotary switches on the front face of the TS trip system.

The protection settings and alarm settings can be read by EcoStruxure Power Commission software, and EcoStruxure Power Device app.

The settings are displayed with:

  • EcoStruxure Power Commission software

  • EcoStruxure Power Device app

Setting the Ir Pickup

The Ir pickup setting value is expressed according to the rated current In.

WARNING
HAZARD OF FIRE
  • It is recommended not to set the long-time overcurrent protection pickup Ir to off.
  • When Ir is set to off, the long-time protection does not protect the system against overload. The instantaneous and/or short-time protections must be set accordingly.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Ir pickup = Ir setting x In rated current.

The Ir setting values are: 0.4, 0.5, 0.6, 0.7, 0.8, 0.9, 0.95, 0.98, 1 and off.

To set the Ir setting to off, follow the instructions below:

Step

Action

1

Open the trip system cover.

2

Rotate the Ir rotary switch in clockwise and set to value 1 by using a screwdriver.

NOTE: Do not use any other sharp tools to rotate the switch.

3

Press and hold the Ir push button using a screw driver. Rotate the Ir rotary switch to off position while holding the Ir push button.

NOTE: The Ir off push button must be pressed and held in order to turn the Ir setting rotary switch to off position.

4

Release the push button. The Ir setting is set to off.

5

Rotate the Ir rotary switch to the value directly to change the Ir setting from off to other settings.

6

Close the trip system cover.

When the current is higher than Isd or Ii, only short-time overcurrent protection and instantaneous protection are operational.

Setting the tr Time Delay

The time delay settings correspond to the tripping times for an overload of 6 x Ir in cold-state conditions.

The table below gives tripping times according to tr time delay.

tr setting

Accuracy

0.5 s

1 s

2 s

4 s

8 s

10 s

12 s

16 s

20 s

24 s

Resulting tripping time at 1.5 x Ir

0 to -30%

12.5 s

25 s

50 s

100 s

200 s

250 s

300 s

400 s

500 s

600 s

Resulting tripping time at 6 x Ir

0 to -20%

0.5 s1

1 s

2 s

4 s

8 s

10 s

12 s

16 s

20 s

24 s

Resulting tripping time at 7.2 x Ir

0 to -20%

0.36 s2

0.69 s

1.38 s

2.8 s

5.5 s

6.9 s

8.3 s

11 s

13.8 s

16.6 s

1: Accuracy 0 to -40%

2: Accuracy 0 to -60%

Predefined Events

The function generates the following predefined events:

Code

Event

History

Severity

0x6400 (25600)

Ir trip

Trip

High

0x6200 (25088)

Ir start (I ≥ 105% Ir)

Protection

Medium

0x0C07 (3079)

Ir protection off

Protection

Medium

Predefined events cannot be modified by the user. For general information about events, refer to Event Management.

Protection events are generated as follows:

  • The start event is generated when the protection picks up.

  • The trip event is generated when the circuit breaker tripping voltage release (MITOP) activates.

Recommended Actions

Code

Event

Recommended actions

0x6400 (25600)

Ir trip

Check the load and reset the device.

0x6200 (25088)

Ir start (I ≥ 105% Ir)

Check the load.

0x0C07 (3079)

Ir protection off

No action required.

Resetting a Trip Event

For information about resetting the circuit breaker after a trip due to an electrical fault, refer to the relevant document:

  • EasyPact MVS1 Circuit Breakers with TS Trip System - User Guide
  • EasyPact MVS2 Circuit Breakers with TS Trip System - User Guide
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?