DOCA0299EN-03

Event List

Event Characteristics

The events are listed according to the history in which they are logged.

Each event is defined by the following characteristics:

  • Code: event code

  • Event: user message

  • History

  • Type: not customizable

    • Entry/Exit: occurrence/completion event

    • Pulse: instantaneous event

  • Latched:

    • Yes: the event is latched and the user must reset the event status.

    • No: the event is unlatched.

  • Activity:

    • Enabled

    • Disabled

  • Severity:

    • High severity events

    • Medium severity events

    • Low severity events

  • Service LED:

    • Yes: the service LED is lit in either red or flashing in red, depending on the severity of the event. Maintenance action is required.

    • No: the service LED is not lit. No maintenance action is required.

  • EPD App:

    • Yes: the event can be displayed on a smartphone with EcoStruxure Power Device app (EPD).

    • No: the event cannot be displayed on a smartphone with EcoStruxure Power Device app (EPD).

Trip Events

Code

Event

History

Type

Latched

Activity

Severity

Service LED

EPD app

0x6400 (25600)

Ir trip

Trip

Pulse

Latched

Enabled

High

No

Yes

0x6401 (25601)

Isd trip

Trip

Pulse

Latched

Enabled

High

No

Yes

0x6402 (25602)

Ii trip

Trip

Pulse

Latched

Enabled

High

No

Yes

0x6403 (25603)

Ig trip

Trip

Pulse

Latched

Enabled

High

No

Yes

0x6405 (25605)

Over temperature trip

Trip

Pulse

Latched

Enabled

High

Yes

Yes

0x6407 (25607)

Self diagnostic trip

Trip

Pulse

Latched

Enabled

High

Yes

Yes

0x641D (25629)

Ultimate self-protection trip (DIN/DINF)

Trip

Pulse

Latched

Enabled

High

No

Yes

0x641E (25630)

Ig test trip with test button

Trip

Pulse

Latched

Enabled

High

No

Yes

0x6433 (25651)

Phase current transformer sensors open circuit trip

Trip

Pulse

Latched

Enabled

High

Yes

Yes

Protection Events

Code

Event

History

Type

Latched

Activity

Severity

Service LED

EPD app

0x03F5 (1013)

Ir prealarm (90% Ir < I < 105% Ir)

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

Yes

0x6200 (25088)

Ir start (I ≥ 105% Ir)

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

Yes

0x050C (1292)

Ig alarm (I ≥ 80% Ig)

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

Yes

0x0C07 (3079)

Ir protection off

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

No

0x0C08 (3080)

Ii protection off

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

No

0x0C09 (3081)

Ig protection off

Protection

Entry/Exit

Unlatched

Enabled

Medium

No

No

0x1519 (5401)

Protection in fallback settings for Rotary switch failure during power on initializing

Protection

Pulse

Unlatched

Enabled

High

Yes

Yes

Diagnostic Events

Code

Event

History

Type

Latched

Activity

Severity

Service LED

EPD app

0x1400 (5120)

Control unit self test major malfunction 1

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1402 (5122)

Internal current sensor disconnected

Diagnostic

Entry/Exit

Unlatched

Enabled

High

No

No

0x1404 (5124)

Control unit self test major malfunction 2

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1405 (5125)

Control unit self test major malfunction 3

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1406 (5126)

Control unit self test major malfunction 4

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1409 (5129)

Unable to read sensor plug

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1413 (5139)

Ig test - no trip

Diagnostic

Pulse

Unlatched

Enabled

High

No

No

0x1414 (5140)

NFC invalid communication #2

Diagnostic

Entry/Exit

Unlatched

Enabled

Medium

Yes

No

0x1416 (5142)

Control unit self test major malfunction 5

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x142F (5167)

Last modification of protection settings has not been completely applied

Diagnostic

Entry/Exit

Unlatched

Enabled

Medium

Yes

Yes

0x151A (5402)

Control unit over temperature

Diagnostic

Entry/Exit

Unlatched

Enabled

Medium

Yes

Yes

0x1434 (5172)

Firmware self diagnostic error

Diagnostic

Entry/Exit

Unlatched

Disabled

High

Yes

Yes

0x150F (5391)

Internal Current Power Supply (CPS) sensors malfunction

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

0x1517 (5399)

Current unbalance > 50%

Diagnostic

Entry/Exit

Unlatched

Enabled

Low

No

No

0x1518 (5400)

Control unit self test major malfunction 6

Diagnostic

Entry/Exit

Unlatched

Enabled

High

Yes

Yes

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?