DOCA0299EN-03

Monitoring the Tripping Circuit

Presentation

When the TS trip system is energized, it provides constant monitoring of the following:

  • The internal tripping circuit

    .
  • The connection of the internal sensors (internal current transformers, sensor plug, performer plug)

    .
  • The connection of the circuit breaker tripping voltage release (MITOP) to the TS trip system

    .
NOTE: The mechanism is not monitored. It is recommended to perform preventive maintenance as proposed by Schneider Electric.

Availability

Monitoring the tripping circuit function of the TS trip system is available on TS 2.0S, 5.0S, and 6.0S trip system.

Operating Principle: Ready LED

A. Ready LED

The result of the monitoring is indicated by the ready LED on the front face of the TS trip system, as follows:

  • The ready LED is flashing green: the internal tripping circuit of the circuit breaker is functioning correctly.

  • The ready LED is off:

    • The TS trip system is not powered.

    • Or there is a detected incident in the tripping circuit.

Circuit Breaker Status

Following the detection of an incident in the tripping circuit the circuit breaker may be tripped or not, depending on the type of incident detected.

Tripping Data and Availability

The following data about the tripping function is logged by the TS trip system:

  • Total number of trips

  • The recent trip cause

The tripping data is available with:

  • The EcoStruxure Power Commission software for last 30 trip records.

  • The EcoStruxure Power Device app through NFC communication.

Predefined Events

The monitoring of the tripping circuit generates the following events:

Code

Event

History

Severity

0x6407 (25607)

Self diagnostic trip

Trip

High

0x6433 (25651)

Phase current transformer sensors open circuit trip

Trip

High

0x1400 (5120)

Control unit self test major malfunction 1

Diagnostic

High

0x1402 (5122)

Internal current sensor disconnected 

Diagnostic

High

0x1404 (5124)

Control unit self test major malfunction 2

Diagnostic

High

0x1405 (5125)

Control unit self test major malfunction 3

Diagnostic

High

0x1406 (5126)

Control unit self test major malfunction 4

Diagnostic

High

0x1416 (5142)

Control unit self test major malfunction 5

Diagnostic

High

0x1409 (5129)

Unable to read sensor plug

Diagnostic

High

0x1518 (5400)

Control unit self test major malfunction 6

Diagnostic

High

Predefined events cannot be modified by the user. For general information about events, refer to the Event Management.

Recommended Actions

Code

Event

Recommended actions

0x6407 (25607)

Self diagnostic trip

Plan to replace the TS trip system.

0x6433 (25651)

Phase current transformer sensors open circuit trip

Plan to replace the circuit breaker.

0x1400 (5120)

Control unit self test major malfunction 1

Plan to replace the TS trip system.

0x1402 (5122)

Internal current sensor disconnected 

Plan to replace the circuit breaker.

0x1404 (5124)

Control unit self test major malfunction 2

Plan to replace the TS trip system.

0x1405 (5125)

Control unit self test major malfunction 3

Plan to replace the TS trip system.

0x1406 (5126)

Control unit self test major malfunction 4

Plan to replace the TS trip system.

0x1416 (5142)

Control unit self test major malfunction 5

Plan to replace the TS trip system.

0x1409 (5129)

Unable to read sensor plug

Check connection of the sensor plug and performer plug. If the connection is good but the event is detected again, replace the sensor plug or the trip system.

0x1518 (5400)

Control unit self test major malfunction 6

Plan to replace the TS trip system.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Resetting a Trip Event

For information about resetting the circuit breaker after a trip due to an electrical fault, refer to the relevant document:

  • EasyPact MVS1 Circuit Breakers with TS Trip System - User Guide
  • EasyPact MVS2 Circuit Breakers with TS Trip System - User Guide
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.