Description
TS Trip System
-
Top fastener
-
Terminal block for external connections
-
Lead seal fixture for protective cover
-
Bottom fastener
-
Protective cover (shown open)
-
Internal battery cover (shown open)
-
Screw for internal battery cover (available for TS 2.0S, 5.0S, and 6.0S only)
-
Internal battery (available for TS 2.0S, 5.0S, and 6.0S only)
-
NFC wireless communication zone
-
Connection with circuit breaker
TS 2.0 and 2.0S Trip System
-
QR code to access product information and trip system type
-
Long-time time delay tr
-
Long-time current setting Ir
-
Ir off push-button
-
Instantaneous pickup Ii
-
Sensor plug with the rated current of the circuit breaker
-
5-pin plug for function test and isolation module (under cover)
-
Trip system identification number
-
Trip system type
-
Ready LED
-
Status bar
-
Service LED
-
Instantaneous trip cause LED
-
Long-time trip cause LED
TS 5.0 and 5.0S Trip System
-
QR code to access product information and trip system type
-
Long-time time delay tr
-
Long-time current setting Ir
-
Ir off push-button
-
Short-time pickup Isd
-
Short-time time delay tsd
-
Sensor plug with the rated current of the circuit breaker
-
5-pin plug for function test and isolation module (under cover)
-
Instantaneous pickup Ii
-
Trip system identification number
-
Trip system type
-
Ready LED
-
Status bar
-
Service LED
-
Instantaneous trip cause LED
-
Short-time trip cause LED
-
Long-time trip cause LED
TS 6.0S Trip System
-
QR code to access product information and trip system type
-
Long-time time delay tr
-
Long-time current setting Ir
-
Ir off push-button
-
Short-time pickup Isd
-
Short-time time delay tsd
-
Sensor plug with the rated current of the circuit breaker
-
5-pin plug for function test and isolation module (under cover)
-
Ground-fault time delay tg
-
Test button for ground-fault protection
-
Ground-fault pickup Ig
-
Instantaneous pickup Ii
-
Trip system identification number
-
Trip system type
-
Ready LED
-
Status bar
-
Service LED
-
Ground-fault trip cause LED
-
Instantaneous trip cause LED
-
Short-time trip cause LED
-
Long-time trip cause LED
Test Button for Ground-Fault Protection (TS 6.0S)
Use the Ground-fault Test button to test the ground-fault protection for TS 6.0S trip system.
Ir off Push-Button
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Do not use sharp tool to push the button during setting
Ir rotary switch to off position.
Failure to follow these instructions can result in equipment damage.
|
Press and hold Ir off push-button before turning the long-time current setting Ir rotary switch to off position. For the operation of this button, refer to Long-Time Overcurrent Protection (L or ANSI 49RMS/51).
QR Code
When the QR code on the front face of a TS trip system is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE Landing Page is displayed.
The landing page displays:
-
Information about the TS trip system.
-
A list of menus.
Trip System Identification Number
The identification number PPYYWWDLLLNNNNNMVS1•••• is made up as follows:
-
Serial number of the TS trip system in the format:
-
PP = Plant code (2 alphanumeric characters)
-
YY = Year of manufacture
-
WW = Week of the year
-
D = Day of the week of manufacture (Monday = 1)
-
LLL = Line or machine number (alphanumeric characters)
-
NNNNN = Unique product number manufactured
-
-
Commercial reference of the TS trip system (8 alphanumeric characters): MVS1••••
Trip System Type
The TS trip system X.0 or X.0S type is coded as follows:
-
X.0 indicates the protection functions provided by the TS trip system.
-
S indicates the Standard TS trip system with NFC wireless communication.
-
No S indicates the Basic TS trip system without NFC wireless communication.