DOCA0299EN-03

Event Definition

Definition

An event is a change in state of digital data, or any incident detected by the TS trip system.

Events are time stamped and logged in the event history of each module.

Events are categorized according to a level of severity:

  • High: urgent corrective action is required.

  • Medium: corrective action needs to be scheduled.

  • Low: for information only.

Events can be consulted with:

  • The EcoStruxure Power Commission software

  • The EcoStruxure Power Device app

Alarms and trips are events that require specific attention from the user:

  • A trip is a high severity event generated when the circuit breaker trips.

  • An alarm is an event with medium or high severity.

Management of Events by TS Trip System

The following diagram gives an overview of how events are managed by the TS trip system.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.