DOCA0299EN-03

Presentation

TS Trip System - Overview

EasyPact MVS circuit breakers with TS trip system provide protection functions.

The TS trip systems are:

  • TS 2.0, 5.0

  • TS 2.0S, 5.0S, and 6.0S

Range of TS Trip System

The following table indicates the functions available on EasyPact MVS circuit breakers with TS trip system:

 

TS 2.0

TS 5.0

TS 2.0S

TS 5.0S

TS 6.0S

Commercial reference

MVS15562

MVS15563

MVS15556

MVS15557

MVS15558

Long-time overcurrent protection (L)

Short-time overcurrent protection(S)

Instantaneous overcurrent protection (I)

Ground-fault protection (G)

Neutral protection (N)

Self-diagnosis and ready status indication

Overcurrent prealarm and alarm indication

Ground-fault prealarm indication

Internal fault alarm inidication

Overcurrent & Internal fault trip indication

Protection & Alarm setting change traceability

RMS current measurements

Trip history

Last 1 

Last 1 

Last 30

Last 30

Last 30

Event history

Last 70

Last 70

Last 70

Embedded NFC-EPD smart phone APP

Embedded USB port-EPC desktop software

Firmware upgradable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.