990-91077K-001

Easy UPS 3SFor Internal and External Batteries
10-40 kVA 400 V & 10-20 kVA 208 V 3:3
10-30 kVA 400 V 3:1
Technical Specifications

Latest updates are available on the Schneider Electric website

11/2024

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?