990-91077K-001

Input Power Factor

Input Power Factor – 3:3 UPSs

The values are at a 400 V, 50 Hz load.

  10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
25% load 0.90 0.92 0.93 0.97 0.96
50% load 0.98 0.98 0.99 0.99 0.99
75% load 0.99 0.99 0.99 0.99 0.99
100% load 0.99 0.99 0.99 0.99 0.99

Input Power Factor – 3:1 UPSs

  10 kVA 15 kVA 20 kVA 30 kVA
25% load

0.96

0.97

0.94

0.96

50% load

0.99

0.99

0.99

0.99

75% load

0.99

0.99

0.99

0.99

100% load

0.99

0.99

0.99

0.99

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.